Technical FAQs

Ask a Question

What is the value named "Stored" in parameter "IP Method" in Ethernet port settings of PowerLogic PM5000 series meter.

Stored: Use the static value programmed in the IP Address setup register of Ethernet port settings of PowerLogic PM5000 series meter.
Was this helpful?
What can we do to improve the information ?