Technical FAQs

Ask a Question

Is it possible to do fine tunning on Compact NSX MCCB with Micrologic trip unit 5/6 for long time protection setting by keypads.

Yes, it possible to do fine tunning using keypads to set the long time protection Ir pick-up on a Compact NSX Micrologic trip unit 5/6.
User can set the exact value required for Ir on the keypad (in steps of 1 A).

Please refer the below attached document
Was this helpful?
What can we do to improve the information ?