Technical FAQs

Ask a Question

What are the consituents of TeSys LE1M35*** non-reversing D.O.L starters.

The standard version of TeSys LE1M35*** non-reversing D.O.L  comprises:
> 1 TeSys contactor LC1 K**,
> 1 TeSys thermal overload relay LR2 K,
> 1 green Start button “I”,
> 1 red Stop/Reset button “O/R”,
> 1 yellow operating indicator.
Was this helpful?
What can we do to improve the information ?