Technical FAQs

Ask a Question

What is the meaning of the "Modbus Serial Connection" port in Full-function Test Kit (FFTK).

This "Modbus Serial Connection" port in FFTK is used to connect this kit to PC/Laptop. You can simply connect this modbus serial connection port to PC by using the serial cable. As this cable is not supplied with the kit, so it is possible to useany available serial cable at your end.

Refer the attached sheet showing the same connection.
Was this helpful?
What can we do to improve the information ?