Technical FAQs

Ask a Question

What is the breaking capacity of the C60PV-DC range MCB at 650V DC.

The breaking capacity for the C60PV-DC is mentioned below:--
 
>> 1.5kA at 800V DC
>> 3kA at 650V DC
Was this helpful?
What can we do to improve the information ?