Technical FAQs

Ask a Question

Is there any workaround to use the powersuite configuration file into new firmware version 2.6 Tesys T relay which are compatible with SoMove software.

Yes, it is possible.

If there is powersuite configuration file (*.impr) is stored on your PC, then open that powersuite file by click on Open with Somove software. After opening software, there is an automatically mesage comes for convering the powersuite file (*.impr) into somove configuration file (*.psx).
Than you can save that Somove configuration file & download in to the new version of Tesys T relay via Somove software.
Was this helpful?
What can we do to improve the information ?