Technical FAQs

Ask a Question

Can the TSXETG100 gateway operate in modbus slave mode to connect a display unit in modbus master mode?

Yes, the TSXETG100 gateway is configured in Modbus master mode by default but it can also be configured in Modbus slave mode. It can therefore be connected to a Modbus master display unit.
To access the serial link parameters, proceed as follows:
  • Start Internet Explorer.
  • In the Address field, enter the IP address assigned to the ETG gateway and press Enter. The default IP address is
  • Enter Administrator as the user name and Gateway as the password. Then click OK.
  • Click on Serial port and set the parameters of the serial port as required.
Was this helpful?
What can we do to improve the information ?