Technical FAQs

Ask a Question

Can the ATV71 drive display LOC or REM on the keypad like the ATV61?

LOC and REM will not show on keypad
Product Line:
Altivar 71
All models and serial numbers
The Altivar 71 drive can be configured to toggle between local and remote but cannot display "LOC" or "REM" on the parameter bar.   
To program one of the function keys to T/K terminal keypad go the command menu 1.6 find F Function key assignments.
example set F4 to TK will allow you to toggle between terminal and keypad modes.
Was this helpful?
What can we do to improve the information ?