Technical FAQs

Ask a Question

Is TesysT sensitive in which way the current flow?

The TesysT can detect in which way the different phase are connected regarding the current flow. You can have an error on the product if you activate the wiring fault. The wiring fault can be disabled or enabled into SoMove settings (go on menu : Settings/Motor and Control/Diagnostic).
Was this helpful?
What can we do to improve the information ?