Technical FAQs

Ask a Question

Could you explain what the parameter FLC1 means ?

FLC1 is used to set the value of nominal current regarding the range of TesysT. For example if you have a TesysT range 8 amps (LTMR08***) and a motor 2 amps nominal current you set the FLC1 to 25% because the current of the motor in this example is the quarter of the full load current here 8 amps. When you put 25% in FLC1 this is means that the current in the register 466 (value of current in percent) take the value of 100% when you reach 25% of the range of TesysT.
 
The purpose of FLC1 is to set the level of current where you are at the nominal current regarding the range of the TesysT.
 
Last example : Motor of 2.7 amps with range of TesysT LTMR27*** so you set the FLC1 to 10% to have 100% in the register 466. We create this parameter (FLC1) to set all the product and level of thermal fault regarding the nominal current.
 
Was this helpful?
What can we do to improve the information ?