Technical FAQs

Ask a Question

How does the High Speed command work, how I should proceed : use Register number 704 bit0 + 704 bit 6 together? Or one of the two?

When the register 704 bit 6 is used only in two speed operating mode. For all other modes you use all the time 704 bit 0 and 704 bit 1.
 
If you are in two speed mode : you use 704 bit 6 for to control the contactor for low speed and 704 bit 0 to control the contactor for high speed.
Was this helpful?
What can we do to improve the information ?