Technical FAQs

Ask a Question

Is TesysT compliant with Low frequency with a speed drive ?

TesysT can be used on upstream of a speed drive but not on downstream because the internal CT’s are only compliant for a frequency between 47 and 63 Hz.
Was this helpful?
What can we do to improve the information ?