Technical FAQs

Ask a Question

What is the tripping class of the GV2 ME, GV2 P and GV2 RT?

The tripping class for GV2MExx, GV2Pxx, GV2RTxx circuit-breakers is class 10. Class 10 corresponds to a direct on-line motor starting time between 4 and 10 sec. Example of a tripping curve:




 
Was this helpful?
What can we do to improve the information ?