Technical FAQs

Ask a Question

What is the meaning of the B, C, D, K and Z curves for C60 Multi-9 circuit breakers?

Issue:  
What do the B curve, C curve, D curve, K curve and Z curve designations mean on Multi 9 breakers?

Product Line:
Circuit Breakers

Environment:
Applies to the ac rated C60 Multi-9 devices

Resolution:
For C60 Multi-9 devices, ac rated, the following is the meaning of the trip curves:
B curve: 3.2 - 4.8 times amp rating for UL489 and UL1077 (3 - 5 times amp rating for IEC)
C curve: 7 - 10 times amp rating
D curve: 10 - 14 times amp rating
K curve: 10 - 14 times amp rating
Z curve: 2.4 to 3.6 times amp rating
Trip curves are included in the 0860CT0201 catalog. http://products.schneider-electric.us/technical-library/?event=detail&oid=0900892680059c6d

Was this helpful?
What can we do to improve the information ?