Technical FAQs

Ask a Question

What power supplies should I use to supply light curtains?

Schneider Electric guarantees the correct operation of its light curtains if they are powered with the following modules:
  • ABL8RPS24030: Universal 24V 3A
  • ABL8RPS24050: Universal 24V 5A
  • ABL8RPS24100: Universal 24V 10A

The power supply must be chosen according to the consumption of the light curtain to be used.
However, the operation of Schneider Electric light curtains with a power supply other than those listed above is not guaranteed.
Was this helpful?
What can we do to improve the information ?