Technical FAQs

Ask a Question

Can I replace the MES108 Input/Output module by the MES114 module?

Yes, for Sepam 1000+ (series 20 and 40), the MES108 module reference 59645 is replaced by the MES114 module reference 59646.

The MES114 module is installed in its place. The relay will require re-configuration via SFT2841 software to accept the new Input/Output module.

The MES114 module has the following characteristics: 10 inputs, 4 outputs, power supply: 24 to 250 VDC.
Was this helpful?
What can we do to improve the information ?