Technical FAQs

Ask a Question

How can I move from the "demonstration" to the "operation" mode on the SFT2841 software for the SEPAM series 20, 40 and 80?


To move from "demonstration" mode to "operation" mode in the SFT2841 software, follow these instructions:
  • Uninstall the software that is currently installed and reinstall the software (or a later version).
  • During installation, in the window containing the "name", "company" and "demonstration" fields, delete "demonstration" and replace it with the key code consisting of 7 numbers with no spaces, followed by  "-", then the last 2 numbers with no spaces. This key code is on the case of the software CD.
Was this helpful?
What can we do to improve the information ?