Technical FAQs

Ask a Question

Does EBX200 support for all 3 types of DC, AC, and PoE ?

Yes, the Com'X200 can be powered :
_AC 100–230 Vac (±15%), Fuse protection: type T 0.63AE/250V (F1), Power consumption 26W
_DC 24 Vdc (±10%) Fuse protection: type 3.15AL/250V (F1500),  Power consumption 26W
_PoE , Power consumption  15W
Was this helpful?
What can we do to improve the information ?