Technical FAQs

Ask a Question

What is the VA burden on PowerLogic ION Series ION8650 meter Auxiliary Power Supply?

Basically the power of ION8650 meter could be supplied from two sources: voltage input and external power. For meters powered from voltage input connections, power is applied when the voltage inputs are energized. In this case the maximum burden will be 6.8 VA per phase; For externally-powered meters, plug in the connector to the appropriately-rated single-phase AC or DC power source. In such case, the maximum burden is 20.3 VA.
Was this helpful?
What can we do to improve the information ?