Technical FAQs

Ask a Question

Please confirm if C60 UL489 and UL1077 series range MCB are required specific polarity when they are used in DC circuit.

These product are not polarized, so it is possible to reverse the current (exchange +/- polarities) but the DC connection is always from upstream.
Was this helpful?
What can we do to improve the information ?