Technical FAQs

Ask a Question

Is it possible to use  Motor mechanism,  Ground fault module &   Communication option   in CompacNSX MCCB breaker at a same time.

Yes, it is possible to adapt all these option at a time in Compact NSX range of breaker.
1.       Motor mechanism >> Yes possible i.e communicating or non communicating
2.       Ground fault module >> Yes
3.       Communication., >> Yes i.e status communication(on off and trip) and communicating motor mechanism
Was this helpful?
What can we do to improve the information ?