Technical FAQs

Ask a Question

Is it possible to use opposite polarity on auxiliaries ( OF and SD switches) of C60 range of MCB

The OF and SD auxiliary switches are not polarized (Multi9 and Acti9 ranges).
So it is possible to use them without polarity focus. Means it can be used with opposite polarity also.
Was this helpful?
What can we do to improve the information ?