Technical FAQs

Ask a Question

What is the the material of rear terminals of Easypact MVS range of ACB where busbar is fixed.

Please find the reply as given below:--
>> Easypact MVS 800 to 2000 A , material of terminal : Aluminium
>> Easypact MVS 2500 to 4000 A , material of terminal : Copper.
Was this helpful?
What can we do to improve the information ?