Technical FAQs

Ask a Question

Is it possible to use 2 number of iOF auxiliary switch (A9A26924) with iC60N (3 Pole 4 Amp) MCB.

Yes, it is possible the addition of 2 no. of iOF auxiliary switch (A9A26924) on the left side of iC60 MCB.

Please refer the attached instruction sheet showing the specification for the usage of the auxiliaries on iC60 range. So it can be installed as per the instruction given in the instruction sheet.
Was this helpful?
What can we do to improve the information ?