Technical FAQs

Ask a Question

What is the flame resistance for LC1F150 range of contactor.

The flame resistance of the LC1F150 range of contactor is 850*C confirming to IEC 60695-2-1.
Was this helpful?
What can we do to improve the information ?