Technical FAQs

Ask a Question

How to change modbus parameter of advantys OTB modbus module

For the Modbus OTB communicator, the fixed communication parameters are the following:
Mode = RTU
parity = EVEN
stop bits = 1
data = 8

these Parameters are fixed, means no way to change them 

with the rotary wheel you can configure only:
- Slave @.
- Baudrate.

You can't change other parameters.

Was this helpful?
What can we do to improve the information ?