Technical FAQs

Ask a Question

What are the Technical Characteristics of Modbus communication Interface module TRV00210.

The Modbus communication interface module TRV00210 is a communication interface which allows intelligent modular units (IMUs) in the ULP system to communicate using the Modbus protocol.

Please find the Technical characteristics for TRV00210 in the below attachment.

Was this helpful?
What can we do to improve the information ?