Technical FAQs

Ask a Question

What are the Minimum voltage rating of Acti9 RCDs.

The Acti9 RCD devices are compliant with the standards (IEC/EN 61008 & 61009) that means -10% - +5% of nominal voltage. 
 
In our Acti9 offer: 
- iID 2P 230V => Min voltage = 175V 
- iID 4P 400V => Min voltage = 240V 
- Vigi iC60 230/400V => Min voltage = 205V 
- Vigi iC60 130V => Min voltage = 110V
Was this helpful?
What can we do to improve the information ?