Technical FAQs

Ask a Question

How to program PT ratio as 33000V on primary in PM800 series meter.

In PM800 PT setup it is possible to enter the scale value as x1 , x10 , x100.

This scale value is due to the fact that the value of the primary is limited to 32767.

So user can use scale value x10 ( 3300 ) or x100 ( 330 ) in the PT setup.

Was this helpful?
What can we do to improve the information ?