Technical FAQs

Ask a Question

Is Breaker Mismatch protection (VDC) available in Masterpact NW ACB.

Yes, Breaker Mismatch protection (VDC) available in Masterpact NW ACB.

Mismatch protection ensures that a circuit breaker is installed only in a chassis with compatible characteristics. It is made up of two parts (one on the chassis and one on the circuit breaker) offering twenty different combinations that the user may select.
Was this helpful?
What can we do to improve the information ?