Technical FAQs

Ask a Question

What are the characteristics of Masterpact ACBs at an altitude higher than that of 2000 meters.

For Masterpact Devices , at altitudes higher than 2000 metres, the modifications in the ambient air (electrical resistance, cooling capacity) lower the following characteristics as follows:

User-added image
Was this helpful?
What can we do to improve the information ?