Technical FAQs

Ask a Question

How can manual override of an automatic control system be implemented?

There are many instances where it is necessary to have automatic control of a motor and also the provision of a manual override.
 

  • A typical automatic control utilising contact S1 (the process monitoring contact e.g. thermostat, float switch, limit switch) to control a contactor (coil KM1) to switch a motor is shown below;



 

  • In order to implement manual override, a three position selector switch; S2 (e.g. Schneider Electric Harmony type ZB4BD3 + ZB4BZ103) is utilised as shown in the circuit diagram below;





The 'stay put' selector switch has 2 qty N/O (normally open) contacts;
 

  • The N/O contact in position 1 ('Auto' control) is wired in series with contact S1 to enable automatic control.
  • The N/O contact in position 3 ('Manual' control) is wired in parallel with contact S1 overriding the automatic control and therefore maintaining the operation of the contactor.
  • The centre position (2)  provides a manual 'off'  selection as both N/O contacts are open in this position.
Note: The term 'Hand' control is often used in place of 'Manual' control, such that this arrangement is either referred to as 'Auto - Off - Manual' or 'Auto - Off - Hand'  control.
Was this helpful?
What can we do to improve the information ?