Technical FAQs

Ask a Question

What is the modbus register for peak Demand value for Apparent Power (kVA) in PowerLogic PM850 meter.

Register 2184 is the Peak Demand value for Apparent Power (kVA); it can be viewed at VAd peak on the front panel; Two values are the same.
Was this helpful?
What can we do to improve the information ?