Technical FAQs

Ask a Question

Is it possible using FFTK (Full Function Test Kit) to test the micrologic 6.0?

The FFTK kit is compatible with Micrologic 6.0, if the FFTK firmware version is 1.25.
Was this helpful?
What can we do to improve the information ?