Technical FAQs

Ask a Question

How can I modify the preselection value of a counter or time delay of a TSX MICRO or TSX PREMIUM from a Magelis XBT?

Use the following procedure:
  • Write to a %MW from the XBT.
  • Then, using the program in the PLC application, transfer this word to the %yxxx.P.
Where y = C (counter) or T (Timer) and xxx = number of the counter or the time delay.

Example :%Cxxx.P:=%MWxxx
Was this helpful?
What can we do to improve the information ?