Technical FAQs

Ask a Question

What is the Service Life of integral LED (such as ZBV***) in Harmony XB4 & XB5 range.

100,000 hours is an average lifetime at 25 degrees C and for all colors of integral LED (such as ZBV***).
If Led's are used in good conditions of voltage, vibration, moisture.... they could reach 200,000 hours easily at 25 degrees C.
Was this helpful?
What can we do to improve the information ?