Technical FAQs

Ask a Question

Why ATV71Y HHP (>= 90kw) do not have integrated DC Choke.

ATV71 690V HHP series do not have integrated DC Chokes. That's why a line AC choke is mandatory. This is a technical choice because 690V networks are more perturbated thus AC chokes provides a better protection of input components (compliance to IEC/EN 61000-4-12).
Was this helpful?
What can we do to improve the information ?