Technical FAQs

Ask a Question

What is the replacement for Berger Lahr VRDM motor part number VRDM3913/50LWB (Material number 52627035200).

The Berger Lahr VRDM3913/50LWB motor with material number 52224035000 is replaced by the Schneider Electric BRS39BW460ABA motor.

Refer to complete VRDM39.. to BRS. Cross reference list as attached.
Was this helpful?
What can we do to improve the information ?