Technical FAQs

Ask a Question

What are the part numbers of Fast-acting fuse for Altistart 48 Soft Starter range.

 Refer to attached document of Type1 & Type 2 coordination chart of Altistart 48 ranges; in which Fast-acting fuse part number for Altistart 48 Soft Starter range are available.

Was this helpful?
What can we do to improve the information ?