Technical FAQs

Ask a Question

What are the technical specifications of Samwha EOCR 3CT and SR-CT.

The technical specifications of EOCR 3CT and SR-CT are given below

3CT:

Features

> Fitted to EOCR relays for Large Amp Motor Protection
> 1.0 Measuring Class

SR-CT:

Features


> Fitted to EOCR relays for Large Amp Motor Protection
> Satisfied with IEC Inverse Trip Characteristic

For more information please refer the below attached file

Was this helpful?
What can we do to improve the information ?