Technical FAQs

Ask a Question

How can a Reflex iC60 be incorporated in a centralized management application (building, lighting, etc.).

The Reflex iC60 can be implemented to centralized management applications via the Ti24 interface in the case of an environment with
a PLC or a remote I/O module operating with a control voltage of 24 Vdc.
It is possible to use the iMDU auxiliary if the voltage in use for the centralized management PLCs is different (24 or 48 VAC/DC).
Reflex can also still be controlled from a 230 Vac PLC interface via its two inputs Y1 and Y2.
The operating mode chosen should be most appropriate in relation to the options adopted for operation of the application
(centralized mode with or without local controls accessible in a public area or in a reserved area).
Was this helpful?
What can we do to improve the information ?