Technical FAQs

Ask a Question

Is the NSX Micrologic LTU Software compatible with Windows 7 operating system and above.

The LTU software for Masterpact, Compact NS, Compact NSX Rev 8.0.1 is available on SE website (schneider-electric.com) which is compatible with windows 7. 
 
The restrictions for the software is: the screen size fixed to 100% on Windows 7. 
 
Was this helpful?
What can we do to improve the information ?