Technical FAQs

Ask a Question

Is it possible to set the time delay between 5 to 10 seconds in Compact NSX Insulation Monitoring Module (LV429459).

The time delay of the insulation drop cannot be adjusted in  Insulation Monitoring Module (LV429459). It is comprised between 5 to 10s.
Was this helpful?
What can we do to improve the information ?