Technical FAQs

Ask a Question

Is it possible to communicate the LUCB control unit of TeSys U with modbus communication module via SoMove Lite software.

So-move Lite is a configuration tool that can communicate through Modbus port of a multifunction module LUCM control unit only and not with LUCB control unit or COM module. 
So-move will not communicated with Modbus communication modules like LULC031/ LULC033. 
LULC031/LULC033 is done to make TeSys U communicate with a master, not to communicate with a configuration software like powersuite, it is different even if the way to communicate in both sides is Modbus protocol. 
Was this helpful?
What can we do to improve the information ?