Technical FAQs

Ask a Question

What is the DC burden value of Control Power for PM5100/PM5300 meter.

The correct specification for the DC burden value for PM5100/PM5300 meter range should be "4W max at 125V DC". 
 
Was this helpful?
What can we do to improve the information ?