Technical FAQs

Ask a Question

What is the Quick Start Checklist while installing Ethernet communication card PM8ECC onto a PM850 meter.

 Quick Start Checklist :
> Using the Power Meter display, verify the Power Meter is running firmware version 10.600 (OS, RESET, and DL). Upgrade the firmware if necessary.
> Remove control power and any other power sources to the Power Meter.
> Turn off all power supplying the equipment in which the PM8ECC is to be installed.
> Attach the PM8ECC to the Power Meter.
> Wire the serial port and plug in the Ethernet cable.
> Return control power to the Power Meter.
> Configure the Ethernet communications settings with a web browser (using an Ethernet crossover cable) or with the Power Meter display.
> Configure the serial ports.
> Configure the device list.
Was this helpful?
What can we do to improve the information ?