Technical FAQs

Ask a Question

How I connect to STBNIP2212 if I forgot the IP

 Use clear IP to clear the stored IP in the module by following below procedure.
The lower (ONES) switch is set to one of the CLEAR IP positions to clear both the NIM’s IP parameters and stored device name from Flash memory and no IP address is assigned. The module then waits for a new IP address assignment via available methods. Set the switches in accordance with your system and network requirements and repower the module.
 
 
Was this helpful?
What can we do to improve the information ?