Technical FAQs

Ask a Question

How can I compare two Unity Pro applications for M340, Premium, Atrium and Quantum automation platforms?

The "Unity Dif" application comparison software tool is specially designed for this purpose.
"Unity Dif" allows you to compare two Unity applications generated by Unity Pro and automatically draw up an exhaustive list of all the differences.
"Unity Dif" is an option in the Unity Pro Extra Large programming software. 

"Unity Dif" increases productivity during the main life phases of a control system:
  • Application design and debugging
  • Startup of installations and processes
  • Operation and maintenance of installations and processes

"Unity Dif" is an efficient tool for handling Unity applications for:
  • Control system design offices
  • Operation and maintenance managers
  • Installers and systems integrators.
Was this helpful?
What can we do to improve the information ?