Technical FAQs

Ask a Question

What is the actual temperature on the heat sink if the ATV61 or ATV71 drives thermal is showing or reading 118%?

Issue:
What is the actual temperature on the heat sink if the ATV61 or ATV71 drives thermal is showing or reading 118%?

Product Line:
Altivar ATV61 ATV71

Environment:
All

Cause:
Wants to know how hot the heat sink is getting when the drives thermal is showing 118%

Resolution:
Approximately 100 degrees C
Was this helpful?
What can we do to improve the information ?