Technical FAQs

Ask a Question

What is the MTBF values for ABL8RPS24100 power supply.

MTBF will depends on the main power supply as these ABL8 power supplies may have the input voltage range from 100...120 V AC single phase [terminal(s): N-L1] or 200...500 V AC phase to phase [ terminal(s): L1-L2 ]. 

When working at 100% nominal load , MTBF of ABL8RPS24100 at 40°C ambiant temperature is below : 

At main power 220V: 33330 hours 
At main power 500V : 29600 hours 
Was this helpful?
What can we do to improve the information ?